Other Parts Discussed in Thread: FDC2214
Dear Sir/Madam,
In one of our project we are using FDC2214EVM evaluation Board.
There are 4 channels CH0, CH1, CH2 & CH3.
We are inserting capacitor with known value in CH2 and CH3 to detect proper capacitance value using GUI.
Firstly we are using only CH2, then the value observed in GUI is having +2% tolerance
For 62pF Capacitor, in GUI we observe 64pF capacitor.
Then if we are using only CH4, then the value observed in GUI is having +4% tolerance
For 62pF Capacitor, in GUI we observe 66pF capacitor.
So therefore the value is different for different channels.
How to achieve same value in two different channels with similar tolerance or less tolerance?
Please lets us know for any design consideration changes.
Regards,
Kruthi