Other Parts Discussed in Thread: FDC2114,
Hi
I am developing a liquid level system. Trying to understand readings from the FDC2114 EVM. I have found the following. If i connect a 470 pF capacitor across the Channel 3 pads (IN3A and IN3B) on the FDC2114 EVM, i get a result for the sensor capacitance of 450 pF - sort of OK. If I connect the same cap across the IN3A and ground pins, i get a result of 180 pF. I have changed the CLOCK_DIVIDERS_CH3 register to 0x2001 as suggested on page 42 of the part data sheet. This seems to make no difference. What am i doing wrong?
The sensor in the application is a tube with a rod down the centre - the tube needs to be grounded - hence the single ended configuration. It also has a v simple processor, so i am assuming that the capacitance value will proportional to 1/Datax^2 - correct?
Any help would be very welcome.
Regards
Andrew