Hello,
I have 4 different versions of the DRV5053 (CA, PA, EA, VA) through hole TO-92 package. I have connected them on a breadboard according to the Data Sheet ( http://www.ti.com/lit/ds/symlink/drv5053.pdf ) Page 12, 8.2.1 Typical Application With No Filter
I get a constant ~0.6 V on the output pin with no change when I move a very strong neodymium magnet directly over the sensor. (Very close and all orientations of the magnet)
K & J says that I should get 446 Gauss or 44.6 mT at 0.5" distance.
I see no change on my DMM or on my scope. On the scope I have less than 0.1V of noise even when waving the magnet all over the sensor.
I checked the current and I'm getting 2.7 mA.
I have the .01 uF cap across VCC and GND.
I even tried to flip the IC around to make sure that I didn't have it hooked up incorrectly. That caused the output to go to VCC, so I'm pretty sure that I had it correct the first time.
What in the world am I doing wrong?