Other Parts Discussed in Thread: DRV5013
Hello,
Regarding to the DRV5032, my customer is asking some question.
They will use for position sensor of BLDC.
(Question)
(1) They will consider 7V(max) as the absolute maximum rating.
In this case, is there any problem?
(2) Can this device use for position sensor of BLDC?
(Their BLDC information)
・10 poles, 3000rpm(max)
Regards,
Tao2199