Other Parts Discussed in Thread: DRV5055, DRV5056, DRV5055-Q1
I'm working on a project to sense magnetic fields and record the field strength. Previously, I used the HMC5883L magnetometer shown in the link below to measure the field through I2C:
www.adafruit.com/.../1746
However, the magnetic field that we're trying to sense is 10 teslas, which the HMC5883L cannot handle without saturating. Once the device saturated, we had to reset it, and this occurred every hour. So I'm looking for a replacement.
I found one product, the DRV5053, and I was wondering if it can handle 10 teslas safely. The datasheet showed that it can handle an unlimited magnetic flux density, but I wanted to ask to make sure. Also, are there any other suitable products that can measure the magnetic field and communicate to a small single-board computer through I2C? The DRV5053 doesn't have that capability, and it is definitely necessary in order to take and record measurements through my computer, a Raspberry Pi Zero. To be clear, I want to measure and record the magnetic field so that I can visually graph it and monitor its intensity.
Also, would the DRV5055 or DRV5056 be worth considering here? Both products seem relatively new, and I'm worried that they might not work in a 10 tesla field.