Hello,
Im thinking of using the DRV425 to measure magnetic fields in the surroundings.
The device should distinguish between earths magnetic field and magnetic fields from 50/60Hz power distribution.
The later is typically much smaller than earth magentic field.
This device will have a position to measure DC-fields and a postiion to measure AC-fields from 50/60HZ equipment below say 150Hz (I dont need harmonics)
I would like to have multiple measuring ranges bij switching/bridging multiple shunt resistors.
Switching these would ideally be done by an MCU based on the ERROR and/or OVERRANGE pins of the DRV425.
My question is could i use for instance a MOSFET (with known Rdson) to switch the shuntresitors?
Furthermore:
Im using a second order low-pass filter (Fc approx. 150Hz) amplifier circuit after the DRV425 to amplify and filter the DRV425 noise.
Would this be adequate to measure a 100nT field with some sort of accuracy (say +/-20%)
Any tips on how to filter the DC component (due to earth magnetic field) from the DRV425 signal?
Ideally this will be switched on and of with an signal from the MCU.
Any input would be greatly appreciated.
Thanks in advance
Bas