How orthogonal is the sensing direction to the top/bottom of the sensor? What is the parallelism of those two sides?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How orthogonal is the sensing direction to the top/bottom of the sensor? What is the parallelism of those two sides?
Hello Nathan,
Unfortunately I do not have access to manufacturing tolerance data. That being said, if I look at the die size inside the package and presume the worst case scenario of the die being all the way down on one end and raised to the maximum level on the solder on the other end then that would create about 0.6° of tilt from the package floor where the die is attached. However, this is an estimate of a worst case scenario, and it will usually be much better than that. It is also important to note that from some brief testing that I did, the error from this tilt would be roughly 0.3mV on the output, which is minimal compared to the combined errors from sensitivity variance/errors and noise.