Hi Team,
I have a question on the Bus Bar Application Magnetic Field Calculator for the DRV425. Understand that each DRV425 saturates at 2 mT, so the system should be designed to keep the magnetic field below this value. However, in the calculator tool mentioned above the Differential Magnetic Field (Bdiff) value turns red if it exceeds 2 mT.
Can I get some clarity on if this value also needs to remain under 2 mT or is it only the two individual sensor magnetic fields that I need to pay attention to?
Thanks,
Mitchell