I have two CC2650 sensortag's to be used in a cigar humidor monitoring project.
As new I checked the calibration of the Humidity sensor with a Boveda 69%RH humidipak, one of the sensortags showed a steady 69%RH and the other one was a 67.5%RH. Close enough and within spec of the HDC1000 -sensor.
I've had one of the sensortags in a humidor for more than a week now. The humidity seemed to rise a few %. per day which I thought was odd as the analog humidity meter in the humidor was showing a steady 65-70%RH. I took out the sensortag from the humidor when the reading was reaching 78%RH. Strange thing is that it doesn't drop down below 33%RH even after hours in the same space as the other sensortag, which is showing a steady 18%RH. The temp readings are within 0.1 degrees C between the sensortags.
It seems that the humidity sensor starts to drift quite rapidly when operated in humid conditions, what started as a RH difference of 1.5%. between the sensortags is now a 15%. difference in RH.
Has anyone else had similar findings with the HDC1000? Do I possibly have a defect unit?
Cheers,
Mikael