HDC1080 can used in Detection of soil moisture ?
application in soil,test the temperature and humidity。
if no,can you help to recommend suitable products?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HDC1080 can used in Detection of soil moisture ?
application in soil,test the temperature and humidity。
if no,can you help to recommend suitable products?
Hi Roy,
I suppose that there is no problem to use the HDC1080 in soil moisture detection: the only precaution could be to avoid direct contact of the sensing element with the ground .
Can you give us more details on the application, so that we can figure out if there are other side effects?
Best regards,
Carmine
Hello Carmine,
I have the some question, I have a customer that need to measure soil humidity. (Expected volumes: 20K per year).
please refer to this picture as reference:
Can you please advise if there is a possibility to measure soil humidity with the HDC1080 like the above setup
If not, can you please recommend me device that can implement this kind of application .
Thanks in advance
BR
Shai Berman