Dear Community,
I am trying to implement the LMP91000 for a dissolved oxygen probe (2 wire) that requires ~670 mV bias. I am using a Cypress PSoC MCU with their internal VDAC at 3360 mV driving into VREF of the LMP91000. I intend to use the PGA at 20% to get me to 672 mV final. I am currently trying to test my setup and I'm getting some weird results. Firstly the VDAC out is reading 3358 mV when unconnected to anything, but once I connect it to the VREF on the LMP91000, i get 1353 mV at the pin on the PSoC. Vout on the LMP is giving me the same value.
My settings are as follows:
LMP91000_TIA_GAIN_EXT | LMP91000_RLOAD_10OHM,
LMP91000_REF_SOURCE_EXT | LMP91000_INT_Z_50PCT | LMP91000_BIAS_SIGN_POS | LMP91000_BIAS_20PCT,
LMP91000_FET_SHORT_DISABLED | LMP91000_OP_MODE_AMPEROMETRIC
Can someone help me locate my 672 mV?