Hi,
The datasheet says that "the heater is an integrated resistive element that can be used to test the sensor".
If we want to test the sensor, how should we use the heater function?
Best Regards,
Kuramochi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The datasheet says that "the heater is an integrated resistive element that can be used to test the sensor".
If we want to test the sensor, how should we use the heater function?
Best Regards,
Kuramochi
Hi Kuramochi-san,
If you switch on the heater, you can see that the temperature output will increase of 1 or 2 degree C, and the relative humidity will decrease of about 5 to 10% of its current value.
This can be used as self test for understand if the device is working or not.
Please let me know if you have any doubts or need further information.
Best regards,
Carmine