We want to verify if the reading data is correct or not for increasing reliability of data communication.
The acquisition of both temperature and humidity is assumed.
Our considaration is as following.
1. Is the sequence correct? (Of course, the setting data to register could be optional)
2. Could we repeat reading data from the register without triggering next measurement?
The purpose is the comparison of the reading data.
BestRegards