Dear Expert
I have a question about HDC1080.
In the HDC 1080 used by my customers,
Variations in output accuracy are confirmed.
There are two kinds of boards on which the HDC 1080 is mounted.
'' Substrate with problem in accuracy '' '' Substrate prepared for replacement ''
Even though the two boards are designed and manufactured with exactly the same pattern, outline and measurement conditions
There is an error in humidity detection accuracy regardless of it.
Think of factors of temperature offset from past threads,
Layout etc. are exactly the same, other factors are considered.
E2E: http: //e2e.ti.com/support/sensor/humidity/f/985/t/517761
Below is a table of measured values attached, but calibration
Attached is the data of the ideal value and measured value that I went through.
Despite the fact that the accuracy of temperature is almost flat, only the accuracy of humidity,
There is a big error in the plus direction.
I am staring that there is an error in humidity due to factors other than Temperature Offset,
Please tell us your views.
Best,Regars
FukazawaHDC1080 Measurement result.xlsx