Hello,
Customer wants to use HDC2010 to sense the temperature and humidity of environment. Out side of system, not system inside.
End Equipment is LTE Module and board layout and case are as attached. PCB size is 4.5 x 6.
In attached picture, RED area is for Antenna so cannot locate HDC2010 and cannot make ventilation hole in the case, either.
To sense the temperature and humidity of outside of system, where is the best location of HDC2010 and how she can make ventilation hole. (Hole size and the counts of hole.)
If there is no space to locate it on PCB, how she can use HDC2010?
Could you recommend the location of HDC2010 and the ventilation hole spec?
Regards,
Nicky