Question 1:Our application is more special, may be long time exposed to high humidity environment, HDC1080 deviation of 15% is too high, if there are other IC or any solution to solve the problem of the high humidity environment
Question 2:If the IC accuracy can be deviated by exposure to high humidity, how long the IC can achieve normal accuracy after the normal humidity is restored.