Other Parts Discussed in Thread: HDC2010
Hello there,
I have the following problem. I have some devices placed "in the field". This is only a prototype and I have no way of physically debugging them for a while. Each device has a HDC1010 to measure temperature and humidity. In the end those 2 variables are sent to the online server. The problem is I can see only the last measurements for now, which makes the debugging even harder.
The issue: one of the devices keeps returning humidity equal to 0 for a while now. Its temperature is changing normally. It was raining not so long time a go I believe, since the other sensors all show humidity 100 %. My question is:
Is there any faulty condition for the HDC1010 device, when it will return humidity register equal to 0, or will not return anything through I2C at all?
I believe the device is not broken, since it keeps returning proper temperature values. I would appreciate all help in this matter.