Other Parts Discussed in Thread: TMP116
I was looking on HDC2010, can it be that this sensor has a +-0.2 Accuracy (page 5) while having Repeatability of +-0.1c?
For ex the Repeatability of SI7021-A20 which has the same bit resolution and also is a humidity and temperature sensor is 0.01cRMS (page 9 in the SI7021-A20 data sheet)
is the +-0.1c is the same as 0.01cRMS?
or
is the +-0.1c a tipo?