Dear TI,
I see different references to the LDC1000 on measuring different types of metal. Do you have additional application notes or information on this subject?
-Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI,
I see different references to the LDC1000 on measuring different types of metal. Do you have additional application notes or information on this subject?
-Jason
Hello Jason,
Are you interested in metal identification/ Could you please describe the application in more details, and we will be glad to help.
Specifically I would like to see what data TI has for measuring different types of metal. For example, comparing steel to stainless steel. My understanding is that the LDC1000 is able to measure the conductivity of the metal so it should be able to determine the differences but was hoping for data related to this type of measurement.
Thank you for your feedback,
Jason
Hello Jason,
Yes, we have data that shows a clear difference for different kinds of metals.
There are many types of steel and stainless steel, so I cannot know if the ones you target to measure have different resistivity. If they do, you will distinguish them. If they are the same - no.
There is an EVM kit available. I suggest you to request one and perform a quick and simple test!
Hello Michael,
I would take Rp Measurements of known large targets at a fixed position from the coil, and plot them (Ro data) as a function of conductivity of those targets.
Then I'd have a look-up table/fit function, so I could measure unknown metals.
Hi Natallia,
I want to detect metal composition. The sensorcoil-diameter should be as small as possible for this appilcation.
Best regards,
Michael
Hello Natallia Holubeva,
I want to test the resisivity of procedure of the liquid metal transforming to solid metal ,the temperature is -50°C to 50°C, I want to plot the resisivity line with