Hi,
It is said that the source code of LDC1000EVM will be released recently. Is that ture? When will it be released? Where can we get the source code?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
It is said that the source code of LDC1000EVM will be released recently. Is that ture? When will it be released? Where can we get the source code?
Hi Murali,
Thanks for the answer.I was using the older version before, and there is no firmware folder in it. I find the active code after re-installing the new version. Thanks again, and I will ask again when encounter some problems.
Hi Murali,
There is another question. From the Technology Documentation, we can see the application example as follow:
As the picture shown, we can see that in this application there is only one piece of LDC1000 chip and one capacitor, but with two pieces of inductance circuit. My question is coming. In the practical application how to connect the two inductance circuits into one LDC1000 chip? Or whether the picture is just a simplification, and it will need two LDC1000 chips in practical application? Thanks.
Hello Peng,
Please refer to the Analog Wire Blog:
Best Regards,
Natallia Holubeva