This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Coil design verifying

Hi

In our application we need to determine the best coil design in our setup with given parameters.

We have 4 coil designs, and we want to measure changes in distance between the coil and a metal target with the highest precision, but if we could go with a small metal target that would be benefitial due to space limitations.

We have made 4 four stainless steel disks of different diameters to be tested with the 4 coils. They are 15mm, 20mm, 30mm and 40mm. The coils are in the range 35 to 40mm i diameter.

Are there any guidelines which explains how I go about to determine test criterias and endpoints in my testing?

In the case where all coils react to all metal disks what do I do check wether one disk/coil configuration provides better resolution, linearity or range than another configuration?

If anyone has any experience or insight to help me it would be greatly appreciated!

  • Hello Bjornar,

    For the best resolution, the rule of a thum is for the coil diameter to be the size of the target. The useful range would be 1/2 of the diameter of the coil you are using. For example, if your coil is 40mm, the endpoints would be the closest distance as the starting point and around 20 mm as the end point.

    You can see from the GUI response what set up provides you the best resolution. I would advise to log the data in a text file and do plots for all the possible set ups to determine which works better. From the logged file, you can see the 'raw data' of L and Rp and plot it versus the distance.

    I assume you are using only L measurement, but could you please confirm?

    Please, feel free if you have any questions.

    Best Regards,

    Natallia Holubeva

    Application Engineer

  • Hi Natalia

    We will go with a solution which is in accordance with the rule of thumb as you suggest, but we have to verify the correct sizes in testing.

    I am actually a bit uncertain of how I use the GUI response to check resolution and to see which works the best. Will I have to check the total raw data change (startpoint value minus endpoint value) for each setup, and if this change is bigger in some cases then that means a better resolution?

    How do I determine wether to use the Inductance or the Rp? The target is steel, does that matter?

    Regards, Bjørnar

  • Hello Bjornar,

    The use of either L or Rp is usually determined by the application. For some applications, you might use both (for example, if you are trying to determine the composition of the metal). In your case, you are trying the sense the distance only, correct? I would suggest using L measurement since it is sufficient in this case. Additionally, L measurement is more stable with temperature drift. What is the frequency of your sensor?

    In the GUI response, your assumpions are correct. Please, proceed as you stated above.

    Best Regards,

    Natallia Holubeva

    Application Engineer

     

  • Will L give the same resolution as Rp? It seems as the response in the GUI is much lower for the inductance.

    Why is the L measurement more stable? Due to resistivity changes in the target material when temp. changes?

    The frequency is around the maximum for the chip, 5MHz.

    Best Regards,

    Bjørnar

  • Dear Bjornar,

    L is stable with temperature variation (~30ppm/°C) since it is dominated by shift in sensor capacitor temperature coefficient. Rp is subject to temperature variation (3900ppm/°C for Cu). The variation is dominated by shift in conductivity of target. For Rp measurement, temperature compensation may be required, which introduces more work for you.

    Your target is steel, but is there a way you could use Aluminum instead? Certain kinds of steel have ferromagnetic properties that may force you to use Rp instead. What kind of steel is it?

    Also, in the GUI streaming tab, please right click on the inductance window and choose 'Toggle Data Type'. You will see the output codes instead of the inductance which you can work with as well.

    Best Regards,

    Natallia Holubeva

    Application Engineer

  • Hi Bjørnar,

    The L resolution is not the same as the Rp resolution; it can be better or worse, depending on the system.

    The L measurement is typically more stable due to the change in conductivity across temperature; for example, copper conductivity changes by 3900ppm/degC, so the Rp would change at that rate.

    For L measurements, the temp-co of the sensor capacitor is typically the dominant source of temperature shifts; this is typically MUCH better. Please refer to the app-note (http://www.ti.com/lit/pdf/snaa212) for more information.

    Regards,

    ChrisO 

  • Hi again Natallia

    I understand, Temperature changes will be a factor so I think we will go for an L measurement.

    We have chosen steel because that gave the best range and resolution in the coil designer. We can absolutely use aluminium, but random testing of aluminium targets shows a much lower response compared to steel but it may be somewhat due to the metals quality. We used an aluminium ruler, a cut off piece of alu. plate from the local aluminium supplier which is probably construction quality.

    Can you verify wether alu. will typically give a lower response compared to steel? The reason we want to optimise the response is that we need to press down the coil and target size in this application as space, size and weight are important design drivers.

    The range we need to measure is 1-15mm and the target size should ideally be in the range of 20-30mm

    On the coil sizes we have a bit more room, but bigger coils than 40mm could cause problems so you see why we need to optimise the design.

    Thanks again for your input to our work.

  • In general, because Aluminum has a higher conductivity, it will produce a larger response than steel.

    The mechanicals you are proposing look fine.

    Regards,

    ChrisO

  • ok, good.

    Is there also a way to calculate/estimate the power consumption of the circuit? The chip uses 1,7mA but we would like to know the total consumption of the circuit with periferal components and the setup described above with a 250 turn, 110ohm coil and 22pF capacitor.

    Rgs, Bjørnar

  • Hello Bjornar,

    The total power consumption of the circuit is the power consumed by the IC itself and the power consumed by the LC tank. The power consumption of the IC is described in the datasheet (you are correct, it is 1.7mA). The power consumption of the LC tank depends on the Q-factor (the larger the Q, the less power it consumes) and the Rp. If you are using the GUI, you are able to select peak-to-peak voltage you are driving the sensor with (1Vpp - 4Vpp). 

    Best Regards,

    Natallia Holubeva