Hello,
we are mounting LDC1000 sensors on a mechanical structure and need to place the target material in front of them.
We used the WEBENCH Design Center Tool to determine the right target material and the result was: SS416 (we know it as 1.4005).
The solution purposed by the tool is difficult to find for us. Can we reach the desired measurement precision also using other materials? If yes, which materials can we use?