Hi, I am working on the prototype of Gear teeth count. My gear thickness is 2-3mm and the distance between consecutive teeth is 10mm. Is it possible to use a coil of diameter 6mm? If I use wire wound as a coil, what are the necessary settings I need to do other than RP_MAX and RP_Min. I mean any frequency settings in LDC is necessary? Can I use series Inductance if my wire wound have less Inductance? what is the normal range of Series Inductance?
Thanks,
Naveen