Hi, I want to know how to increase the distance of inductance sensing for LDC1000, because I have a rectangular PCB Coil (around 220uH with 470p and frequency of 781KHz) with a 50 turn and long of 24cm, wide of 2.3cm to detect a office staple, the best detect distance i can get is around 0.5cm to 0.8cm, seems the radius of a coil would be the detecting distance i should get 1.1cm of detecting distance, is because my coil is a rectangular PCB or because my object staple it too small to detect.