The LDC1000 has no reset pin ,but there is some internal reset circuit anyhow.
I noticed that below 3.6V all SPI registers read as zeroes (0x00)
I noticed too that above 3.8V , the SPI reports nothing special , it all seems to work.
I noticed also some grey zone somewhere between 3.6 and 3.8V where all SPI registers report 1's (0xFF)
Now my question is :
What exactly is the internal behaviour ?
What happens when the VccA is below 4.75V , and yet above the reset treshold? Should we have an extra power supply monitoring in order to get dependable results from the LDC1000?
As we work with an STM8 CPU there is only a brownout detection at 2.7V, the LDC1000 is already permanent in the reset state by then.