The LDC1000 EVM board is connected and functional with the supplied GUI. The sensor does not respond well when positioned near a inductive surface. The configuration settings are the default values which appear to be incorrect. The sensor capacitor is 100 pF, LDCLK is 6 MHz, Rp_MAX and Rp_MIN are both 3926.991 kOhms, sensor frequency 2.5 kHz, Comparitor threshold high and low are both 0. Please supply the all of the setting in which the on-board sensor will perform the best. The TI documentation does not indicate what settings are recommend as the defautls appear to be incorrect when using the supplied EVM board.