I am considering LDC 16xx to use for measuring lift off from and speed of a moving target. I would like to know if that could be done if
1) Target is a carbon steel material is under the influence of a magnetic field.
2) The lift off from the sensing coil would be in the range of 0 - 8 mm
3) There could be some debris (metallic and non-metallic)
4) The carbon steel target is moving at speed from 5 feet/ minute to 200 feet / minute and accurate speed measurement is required.
5) can one channel play dual role of distance measurement as well as the lift off measurement?
I need to evaluate this component for my application. Is there any evaluation kit available?