I'm trying to establish communication to the LDC1614EVM using the breakout that contains the MSP430 Processor. It seems that I continually receive a red light indicator and that the GUI only displays a connection to the LDC 1614 yet the theirs no indication of the inductors being displayed when starting the streaming. Ive connected all the SPI signals and have also included INTB, SD, CLKIN, +3.3V and GND between our pcb and the EVM, the only signal that I haven't brought over is the ADDR signal which is grounded on our board. Could this be the problem? I'm trying to utilize the GUI from the EVM to test our LDC1614 design. Is there any suggestions?
Thanks,
Rick