Dear Technical Support Team,
I have a question about TIDA-00508.
1º Dial demo has 0.1º resolution using LDC1314, so GUI shows xxx.1°.
If it is exchanged LDC161x(28bit resolution), how is the resolution for dial theoretically? (For example, 0.01° or 0.001°)
Customer's application is industrial, so they are interested in how the accuracy is using LDC161x.
Best Regards,
y.i