Hello,
im having a hard time finding the correct filter capacitor value to obtain the 1 Vpp on the cfb pin.
My Setup is as follows:
- LDC1000 eval board
- ferrite coil, L0 = 2,6 mH, ferrite core U67/27/14 (L0 is inductance without target)
- tank capacitor C = 96 nF
- Rpmin = 820 Ohm (measuerd with impedance analyzer)
- Rpmax = 10 kOhm (measuerd with impedance analyzer)
- hence the resonance frequency is somewhere around fres = 10 kHz
In the GUI:
- Rpmax set to 21.547 kOhm
- Rpmin set to 0.798 kOhm
- Sensor frequency set to 10.16 kHz
- Response time set to 6144
- Amplitude set to 4 V
- Sensor Capacitor set to 96000 pF
When i probe the cfb pin, all i can see is 5 V dc. I tried different filter capacitors from 330 nF down to 3.3 pF but all gave me 5 V dc on the cfb pin.
To check my measurment equipment, i used the eval board with its original pcb coil an tank capacitor, here i can see the 1 Vpp Signal, so i assume my scope and probes are fine.
Another thing i recognized is, when i switch between the original eval board and my test setup with the ferrite coil, the field in the GUI that is named "Status: Data Ready (DRDY) Status" changes from "Data Ready" to "Data not Ready".
Kind regards,
Markus Schyma