Dear All,
is it possible to get the pysical properties of the two coils attached to channel 0 and channel 1 of the evm ldc1614 ?
Already known from the chapter about the sensors of the evm in the manual is that the coils has 14 mm diameter , 32 turns and 2 layers .
There are also some plots in the same chapter for which it would be great to get an example how to use them to calculate the register values if possible.
My guess is that you select the frequency of the sensor and take the value for L , Q and Rs out of the plots and calculate everything else from there. Is this correct ?
In the data sheet for the LDC1614 there are plots for a coil with 14 mm diameter , 32 turns 2 layers which was designed for a 1,5 mm thick Aluminum target.
Is it the same coil like the ones attached to the evm ldc 1614 ?
I want to have the data to be able to do the similar thing to the example set up of the ldc in the data sheet. There another coil is used.
The last question I have for know is for which target exactly are the coils designed ?
Thanks for your support in advance.
BR,
Melanie