hi everone
I decided to use TI inductive sensing solution in my design but i am not sure about it.
In my design i have 27 positions . Processor must be able to sense a copper strip reaching at each one of these positions.
This copper strip size is about 40x4 mm2 . This copper strip may contact the positions . In fact this copper strip
glued to a hammer and this hammer impact to each position like playing a marimba the musical instrument .
Each position has a PCB with special shape that must be about 130x8 mm2 .
So with this scheme is it possible to get a coil wire on such a PCB with 130x8 mm2 size for using inductive - Digital converters ?
Is it possible to use one converter for all 27 positions ? If it is possible how can i multiplex them ?
Is it possible to calculate the reaching speed of the copper strip for calculating impact force ?
As i said the copper strip contact to positions . If copper strip contact the coil wire on PCB is it cause any failure ?
If it cause any problem can it be avoided by using a solder mask on PCB ?
Thanks for your support.