I am looking to measure the position of a vibrating magnet (https://www.kjmagnetics.com/proddetail.asp?prod=D201-N52) that is attached to an object that is vibrating at up to 10 kHz. There is a stainless steel plate between the magnet and the pickup coil, which is spaced ~1cm away. The displacement of the magnet is a few microns.
Is the LDC1000 appropriate for this sensing operation? Can it observe motion of a permanent magnet - I know the features say it doesn't require a magnet, but my application requires one for other reasons.
Is this frequency of vibration with small displacement resolvable?
Thanks,
Taylor