Dear Support team,
I'm struggling to find the latest version of Source Code to Evaluation Module LDC1216EVM. There are two revisions for this board, one released in 11-Dec-2014 and a second one in 21-Aug-2015. The second release (rev B) doesn't have an external PLL (CDCE913PW), it has a dedicated 40MHz Oscillator. The source code that I found (packaged on snoc027.rar) is cleared calling a PLL INIT routine to start CDCE913PW and also is dated before August 2015.
Since it is our first time prototyping with LDC1216 inductor sensor and we have used LDC1216EVM to evaluate its use on our business we want to make sure our board is reproducing exactly what evaluation board did before we add our extra code to customize the firmware.
Is that possible to provide the latest source code project used for REV B of LDC1216 evaluation module. This will really help us.
I look forward to receiving your comments.
Thanks in advanced.
Giuliano