Hello,
i have the LDC1101EVM and try to have a good resolution with a high Sample Rate.
The Formula for the conversion time in LHR-Mode is: tconv = (55 + RCOUNT x 16) / fCLKIN
I found the valid range in the description SNOSD01C is : 2 ≤ RCOUNT[15:0] ≤ 65535
So i can calculate the maximum sample rate for RCOUNT = 2 -> 134 ksps with 16MHz fCLKIN and 100 ksps with 12 MHz
minimum sample rate is RCOUNT = 65535 -> 15 sps with 16 MHz and 11 with 12 MHz
So the maximum sample rate with 180ksps is only in RP+L-Mode possible?
But when i open the LDC1101 EVM GUI v.1.0.0.6 and go the LHR configuration i can choose the RCOUNT from 64-1.048.560
so i have a maximum sample rate by RCOUNT = 64 -> 11ksps
and minimum sample rate RCOUNT = 1.048.560 -> 0,7 sps
I have the highest resolution with 1.048.560 ... but it is very very slow ... is that true?
But how can i find out my current sample rate in the gui?
Best regards Jan