Hello,
I am trying to configure LDC1101 for LHR measurement.
In the datasheet (SNOSD01C –MAY 2015–REVISED FEBRUARY 2016) p.42, Table 41, it instructs to set RPMAX_DIS = b0, meaning "Programmed RP_MAX is driven". Shouldn't it be the other way around: RPMAX_DIS = b1, meaning "RP_MAX current is ignored; current drive is off"?
Otherwise, the Rp_max = b111 (Table 41) takes lower value than Rp_min = b101 (Table 41), which violates the setting rule in p.15: The programmed Rp_min setting must not exceed the programmed Rp_max setting.
Please let me know if I misunderstand it.
Best regards,
Minkyun