Dear Sirs
I have a tool made of cast iron which is 50mm thick.
This tool is worn down into 20mm, so I would like to, continiously and very roughly, measure the thickness (4mm accuracy). I will do this measurement once per day, or less.
The tool is exposed to high G-forces and is cost sensitive so an ultrasonic transducer will not work.
I was thinkin about the LDC1612 running at 1KHz.
The measuremen will be done when the tool is at rest.
I saw a formula at the FAQ giving
Maximum thickness we can see through = 503 * sqrt(0.75uΩm / (1kHz *1)) = 13.7mm
So my question is: is it possible or not to measure steel thickness 20-50mm with these components ( or other components) or not accordingly to your expertice knowledge?.
/Dan