Other Parts Discussed in Thread: LDC1612, LDC1614
Hi team,
I have a customer using inductive sensing for proximity switch and interested in our LDC0851.
They need to sense up to 40mm distance, but the max coil diameter is < 40mm (range from 8mm to 40mm). They are testing with our EVM and get < 8mm distance.
In our datasheet, it is recommended that the sensing distance is up to 40% of the coil diameter. Could we increase this to beyond 100% of the coil diameter? Will using multi-layer coil help? And any guide for designing multi-layer coil (they prefer discrete coil than using the PCB).
Is it very critical for the reference coil to be identical to the sensing coil? what is the best positioning for the reference coil and sensing coil?
assuming the reference coil and the sensing coil is identical, what will be the tolerance change with temperature (from -40C to 100C). They need to achieve +/-10% tolerance with all variable (including the tolerance of the coil).