I am currently a student at Texas A&M University. I am seeking a solution for a problem I have encountered in the lab.
Basically, I am looking for a sensor capable of detecting whether a large steel object is or is not present.
The catch is that the sensor and target are separated by up to 2 inches of air.
I would imagine that the most-likely solution would be an inductive sensor. However, I have been unsuccessful in finding a capable sensor.
Specifications are as follows:
- The sensor & the target are separated by up to 2-inches of air.
- No constraints on the sensor technology -- inductive, optical, RF, etc.
- Sensor must work in an environment of periodic rain & dirt.
- A 6.6VDC supply is available to power the sensor.
I would greatly appreciate any suggestions / direction for a solution on my project.
Thanks!
Mitchell