Other Parts Discussed in Thread: LDC1000EVM, LDC1101
Hello,
I bought before 3 days LDC1101EVM inductive sensor, i tried to install the driver (MSP430-Example USB) but the driver is not detected by the windows. i tried to point the windows to search in the software folder and to the development folder but without any result. Then i downloaded the LDC1000EVM software file then the windows detected the driver and the driver is installed with name of (EVM). after that i have run the software GUI for LDC1101EVM but it did not detect the device or any port. Then i tried to run the LDC1000EVM software GUI, the software detected the device but it says the firmware is higher than the required. i attached some photo explain the problem.
please help,
Mohammed