Part Number: LMP8645MKEVAL
Hi,
I am using LMP8645MKEVAL current sensor in my design to check activity on the BUS, My signal frequency is in between 30K to 40K. In burst mode means signal (30KHz) then ideal for some time (10ms) then again signal (30Khz). The bus is at 1.6V DC & AC signal of 30-40Khz is superimposed on this. I am monitoring the BUS by amplifying the signal across the sense resistor but unable to set the gain of LMP8645MKEVAL.
If I use 20K as Rgain then as per graph gain should be 4 but I am getting gain 2. Can you help to fixed the gain in my application.
Sense resistor 29 Ohms, Max Voltage across - 440mV. It will go as low as 200mV I need gain of 4 In my application