Hi,
Now my customer has evaluated LDC1101EVM and measure the sensor frequency with various sensor cap. Then they can see the unexpected behavior when sensor cap is decreased as below.
[GUI setting]
LDC1101EVM GUI Ver.1.0.0.6
LHR mode
L only
[Coil]
Ls : 6.93 uH , Rs:5.90 Ohm
[Sensor cap]
330pF : 3,353,000 count ,2.398 MHz
1,000pF : 2,316,000 count ,1.656 MHz
3,300pF : 14,093,000 count ,10.079 MHz ---> 900kHz was expected but show 10MHz
Can you give your opinion why the 10MHz can be seen with 3300pF? Please let me know if you need more information for other setting.
Best Regards,
Satoshi / Japan Disty