This is Ryo from Japan.
- Question
Can we use coils which have different inductance and design at LDC1X14? From the point of temperature drift, are there any concern?
- Device
LDC 1314 or 1614
- Condition
Four coil are connected to LDC 1X14 devices. Although three coils are almost same inductance, the other coils's inductance is different from three coils. The design of three coils are circle. However, the shape of the other coils is stretched rectangular like A~G below data sheet about reference coils.
http://www.ti.com/lit/ug/snou136/snou136.pdf
- Problem
I found out the value of oscillation frequency is much more different than I expected, every time the LDC1x14 device is reboot. In paticular, at the channel which have 13.8 MHz oscillation frequency at the stretched rectangular coil, the oscillation frequency ls 1 MHz different every reboot.