Dear Sir/Madam,
Not sure if I post at the right place. One of my customer is looking for sensor (<$10 per unit) for automation machines (high vibration and change in temperature)
Travel: 50 mils, +- 0.5 mils
Working temp: -40 – 150 degC
Operating voltage: 5V, or 12V
end application is wire-bonding machine, so the sensor will need to detect the 50 +/- 0.5 mils accuracy along xyz axis.
Can I check TI have any sensor that is suitable for this application?
Best regards,
kpk