Part Number: LDC1000-Q1
Q1.
I would like to confirm the response frequency when LDC1000-Q1 is used in the comparator mode.
In case of LDC0851, "tDELAY Output delay time (Response time) = 580 us (Typ)" in Datasheet Page6 is considered as the response frequency.
In the case of LDC 1000-Q1, "tres (min) Minimum response time" in Datasheet P5 is considered as the response frequency of comparator mode.
Is it correct?
Q2.
The INTB output of the comparator mode is described in the data sheet P13 (Figure 13) of LDC1000-Q1.
I want to confirm the hysteresis of the threshold in this figure.
Could you tell me about hysteresis between Threshold High and Threshold Low?
-Harukawa