Hello,
I have a problem with the connection of the LDC2114EVM.
After connecting it to my PC, the PWR LED, the green LED D11 and the red LED D12 are on.
When I start the "Sensing Solutions EVM GUI", the device gets not detected and also in the "Device Manager" it is not listed. It says "USB-Device not detected"
Switching the port also does not help.
Only when i put the device in BSL-Mode and update the Firmware with the "MSP430 USB Firmware Upgrade Example", the device gets detected and works well.
After unplug and reconnecting it, it does the same things as mentioned and gets not detected anymore.
Another Problem:
When i save the register setings in the register page, and want to write them into the EVM, the values gets updated after a short amount of time and then the old values are set again.
And in general i have problems with setting the registers.
Is there any Problem with the chip?
Thanks for support,
and Kind Regards,
Marcel Kaufmann