Other Parts Discussed in Thread: LDC1614
Dear Forum,
I have been using three separate LDC1614EVM to drive each of my three axes Helmhotlz Coil, and request clarification on the following:
Reference Count 2.4.4 (Using Channel 0)
RCOUNT Conversion Time
0xFFFF 26.2 ms
0x0FFF 1.6 ms
0x00FF 0.1 ms
1. Are these fixed or can I make the conversion time faster or slower and what is the limit ?
2. I am using the Teensy 3.6 micro-controller and wish to drive each of the three LDC1614 to its maximum current (DRIVE_CURRENT_CH0 ) without damaging it, what should the setting be (0x0080 default) in the Current Drive Control Registers ? I’m trying to maximize the magnetic field inside each coil as to increase my signal.
Thank you for your support and please understand that I have been teaching myself how to collect data with micro-controllers.
Sincerely,
Alexander Luis