Hello everyone.
I have made an inductive sensor array, similar to the 16-Button Keypad, (see the documentation TIDU954A) , the following figure is from the mentioned documentation.
The application requires several metal coins to be detected by each coil. The issue faced is the cross talk from other coils. When I select one coil via multiplexer and there are metal coins on other coils, the reading of the selected coil is affected by significant amount.
Is there a way to eliminate cross talks among the coil.
-Sreejit