Other Parts Discussed in Thread: LDC1101EVM, LDC1101
I am testing a combination of LDC1000EVM and Proximity Sensor (OMRON E2C-X10A)
But there is a problem.
Inductance measurement value of LCR meter(sanwa LCR700) and LDC1000 does not match.
<< OMRON E2C-X10A >>
LCR meter(100kHz): 69uH
LDC 1000: 1252uH (Frequency:450kHz, Sensor Capacitor 100pF)
<< Coil printed on board of LDC1000EVM >>
LCR meter(100kHz): 17.4uH
LDC 1000: 19.54uH (Frequency:3.6MHz)
Why is the inductance not calculated correctly in E2C-X10A?
Please tell me if you have any idea.