Other Parts Discussed in Thread: LDC1314, LDC1312, LDC1612,
What are the Amplitude Low Error and Amplitude High Error threshold levels?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The levels are approximately 1.2V and 1.8V respectively. You can refer to the following application note for more information on using the Status register:
Regards,
Luke
Hello,
To clarify:
You can find a deeper description of these error conditions as well as the other STATUS reporting bits in the application note listed above: www.ti.com/.../SNOA959
Regards,
Luke